11/19/2020 12:08 PM | |
Joined: 10/12/2013 Last visit: 1/26/2024 Posts: 28 Rating: (1) |
Hi friends, I tried multiple MRP configuration with 3 SCALANCE X304-2 FE. There are 3 ring. First one is between fiber optic ports of SCALANCE. Second one is for first PLC and ET200M. Third one is for second PLC and ET200M. You can find the topology and settings screenshoots at the attachment. I get error when i try to compile in NetPro. "Only one station can be configured as a manager in an MRP domain. Domain "mrpdomain-1". In scalance settings it allows you to configure multiple ring. But client mode is not supported in multiple ring. So what is the point of having multiple ring configuration of Scalance? Plz help. Attachmentscreenshoots.zip (54 Downloads) |
Follow us on