8/16/2012 11:50 AM | |
Joined: 4/24/2006 Last visit: 6/5/2024 Posts: 8672 Rating: (1158) |
Hello deepak1, Perhaps the following links might help: how do you use the variable symbols defined in STEP 7 with the OPC server of SIMATIC NET? how do you configure an S7 connection for a user application via Industrial Ethernet with the SIMATIC NET PC software? how do you configure an S7 connection via Industrial Ethernet with the SIMATIC NET OPC server and the SIMATIC NET PC software? Best regards, Wizard |
8/16/2012 12:45 PM | |
Posts: 26 Rating: (0) |
Dear Sir, I follow all your link, and i got unsuccess I am using a Belkin N150 Enhanced Wireless Router for connecting S7 controller to my Wireless Network adapter, and i am perfectly connected to Belkin router and my laptop, also i am able to ping CP443-1 from command prompt , the IP of CP443-1 is 192.168.0.1, I also perfectly go online S7 program with Belkin router , The IP of Belkin Router is 192.168.2.1, and the IP of my laptop wireless adapter is 192.168.0.241, also i am able to see all my symbol in OPC scout v10, I just want to see QUALITY GOOD in opc scout, PLZZZZZZZZZ help me, I will be very thankfull for you. |
Last edited by: deepak1 at: 8/16/2012 1:14 PMAll my signal quality are invalid, also my station configurator editor is properly configured, plz help anybody |
|
8/16/2012 1:43 PM | |
Posts: 26 Rating: (0) |
Dear Sir, Plz tell me how to download in PC, because my opc server and and opc scout is installed on same laptop. |
3/27/2014 4:38 PM | |
Posts: 1 Rating: (0) |
Thank you so much Sir! I'm very new, but I hope I can help you one day.
|
11/17/2016 9:05 AM | |
Joined: 9/11/2016 Last visit: 4/16/2024 Posts: 16 Rating: (0) |
I HAVE exact problem but in tia portal v 13 sp1 and set config ethernet addresses with router but i have invalid in opc scout. what should i do ? |
Follow us on