1/20/2015 9:43 PM | |
Joined: 9/17/2008 Last visit: 7/27/2023 Posts: 12 Rating: (0) |
I don't think OB102 is supported by 315-2 CPU |
1/20/2015 9:53 PM | |
Posts: 1058 Rating: (93) |
According to manual it should be supported. Just OB101 is not. See here manual: System Software for S7-300/400 System and Standard Functions Volume 1 and Volume 2 regards |
1/22/2015 4:53 PM | |
Joined: 9/17/2008 Last visit: 7/27/2023 Posts: 12 Rating: (0) |
Not much familiar withwireshark! but do I have to insert OB102 and initialize FB102 inside it, just like OB100? |
1/23/2015 7:29 AM | |
Joined: 3/21/2006 Last visit: 4/25/2024 Posts: 10228 Rating: (1181)
|
And when the communication is not established what is the error/status? Server or client?
|
Follow us on