10/13/2012 10:08 PM | |
Joined: 4/6/2006 Last visit: 2/5/2024 Posts: 604 Rating: (56) |
Hi, What kind of cable do you use? Please check the order number printed on the cable, there are 3 different ones, one for 2,4 and one for 5 GHz. And what is the receiving antenna on the IWLAN/PB Link PN IO's side? If you change the settings on the AP do you also change them on the side of the Link? If not this is soemthing you should do. The cable lengths you use are they based on the RCOax System Manual for 5 GHz?RCoax System Manual If you've checked all this, how is the environment and which 5 GHz do you use? Is it based on 802.11a or on 802.11h? Which channel did you select? Did you check for overlapping APs?
|
Best regards, |
|
10/25/2012 10:38 AM | |
Posts: 3 Rating: (0) |
Hi, It worked... I had to change the setting to 5GHz on IWLan-PBlink side. Thanks a lot for your help.... |
This contribution was helpful to1 thankful Users |
Follow us on