1/13/2014 12:33 PM | |
Posts: 515 Rating: (56) |
hi, No you will not be able to communicate. For communication, you need the same mode/protocol on both the sides.
|
1/15/2014 11:37 AM | |
Joined: 10/18/2012 Last visit: 12/15/2023 Posts: 225 Rating: (23) |
Hello Danish, if you need Panel and PC you can take advantage of Siemens Panel-PCs. It comes with regular Microsoft operating System (i.e. Windows7) and has a Panel already connected to the PC. See this document for example. For Software with Data-Logging there are also packages available that contain: - the IPC, - the Panel - Operating System - HMI-System (WinCC) with data logging. You may find this page useful too. It offers various options of HMI-Software for different quantity of IOs. Note, that the number of "PowerTags" represent the number of variables, that are able to exchange between cpu and the HMI Runtime-Software. For example 512 Powertags as in Package with order-no. 6AV2114-2DA00-0AA0. regards, xnor |
Follow us on