5/5/2022 10:45 AM | |
Joined: 8/3/2009 Last visit: 5/17/2024 Posts: 12970 Rating: (1651) |
Hello Sniki! If you are trying to to accessible devices search or trying to download the HMI with PNIE and search all compatible devices then there is used a DCP Package broadcast, this will work in a local LAN with common switches. But the most third party routers or Access Points do not support DCP forwarding. So I think this will be not forwarded with your AP. -> but you should be able to load the HMI, just use in the Extended Download dialog "Show Devices with the same addresses" or use this one(LINK) you could also use in case of a Comfort Panel Ethernet on both sides instead of PN_IE. If have also a Test environment connected with Wifi, this works also without problems Bye Murof |
If this Information really helps, you could use the Rate function |
|
Follow us on