4/1/2024 2:23 PM | |
Joined: 4/1/2024 Last visit: 4/1/2024 Posts: 2 Rating: (0) |
Dear All, I am using the RTU3031C RTU and I am currently configuring it online via the RTU web server.However, I have noticed it's currently set to be configured via TeleControl Server Basic . Does anyone know how to pre-set the RTU Web server so I can configure it in MQTT rather than Telecontrol? I have shared a screenshot of how the RTU webser looks like ( only allows Telecontrol) when I need it to be as per the example below ( page 34) Connection of the SIMATIC RTU3041C via MQTT to MindSphere (siemens.com) |
Follow us on