5/25/2018 9:35 PM | |
Posts: 7 Rating: (0) |
Hi, I have 2 plc in same network -S7-1500 - 6ES7 511-1AK00-0AB0 - Firmware V1.7 S7-1200 - 6ES7 212-1AE31-0XB0 - Firmware V3.0 Can you help me to put it in work? In S7-1500 always error 80A1 In S7-1200 cant compile bacause do a lot of error. Thanks for help. ------------------------------------------------------------------------------------------ |
Last edited by: Jen_Moderator at: 5/29/2018 7:12:45 AMNew subject after splitting |
|
5/27/2018 11:12 AM | |
Joined: 10/7/2009 Last visit: 8/19/2023 Posts: 266 Rating: (92) |
Dear shadowofgod4343424, Do you copy the MQTT function block from the S7-1200 Example to S7-1500? There are two MQTT Client Application Examples, one for S7-1500 and another for S7-1200, both with the same document (S7-1200 does not support secure communication). Please don't copy function blocks from S7-1200 to S7-1500 or vice vesa, instead download the two examples separately from the below link: For S7-1500 For S7-1200 Best regards, Yu-wen |
Last edited by: Yu-wen Tang at: 5/27/2018 1:47:13 PM |
|
5/29/2018 10:07 AM | |
Joined: 10/7/2009 Last visit: 8/19/2023 Posts: 266 Rating: (92) |
Dear shadowofgod4343424, Here, provide you with a MQTT Client special version for S7-1511-1PN (6ES7 511-1AK00-0AB0) FW 1.7. Since I don't have a CPU of such type, the only thing I can do for you is convert and compile the code without error. Please do the test yourself, if you are still interested. For Error 80A1, it's basically problem with TCP/IP connection. Please check and make sure that the CPU can connect to internet. Please also noted that this version for FW1.7 does not support secure communication, same as the version for S7-1200. Best regards, Yu-wen AttachmentMQTTclient_S7-1511-1_FW1.7.zip (385 Downloads) |
5/31/2018 9:15 PM | |
Posts: 7 Rating: (0) |
Excellent is already working on firmware 1.7. Thanks for all the help.
|
6/2/2018 6:53 PM | |
Joined: 10/7/2009 Last visit: 8/19/2023 Posts: 266 Rating: (92) |
Good to hear. You are welcome. |
6/7/2018 1:38 AM | |
Posts: 7 Rating: (0) |
I, can I change to about 1000 topics to subscribe and about 500 to publish every second is Ok for library? only change size of array’s? Thanks for all |
Follow us on