6/27/2018 4:16 PM | |
Posts: 3 Rating: (0) |
Hi all, I'm trying to do a S7 PUT from a S7-1512 to a IOT2000EDU software PLC via the TIA portal. Attached are the screenshots of the project in TIA portal. I have the PUT block as part of OB1 in S7-1512 and its trying to put the data field "RuntimeMeasurement_DB.MeasuredRuntime" to "DB_RECV.time" in the IOT2000EDU. And this is not working. I don't see the value in the IOT updating nor do I see S7 communication when I do a packet capture in Wireshark. A few things I noticed: 1. One of the S7 communication links under Devices and Networks shows "exists only offline" in the TIA portal. How do I persist this link to the device? 2. I wasn't able to find a flag in IOT2000EDU to enable PUT/GET similar to S7-1512. Is there something like that? Any help is appreciated. Thanks AttachmentPics.zip (17 Downloads) |
6/28/2018 9:13 AM | |
Joined: 6/19/2017 Last visit: 6/12/2024 Posts: 8140 Rating: (165) |
Closed cause question posted twice.
|
My Forum is the place to personalize your profile, |
|
Follow us on