12/12/2016 7:53 AM | |
Posts: 1 Rating:
|
Hi, Over the past two weeks I have had a problem with SCADA WinCC Client. It is installed in our dam system so that our clients can monitor the delivery and consumption of water via WinCC client. Two weeks ago we identified the problem and our clients were not able to access the WinCC client via our static address (Internet Explorer). The initial problem our clients had was loading our Scada site, and they were receiving the following message: Failed to load http://xx.xxx.xx.xxx/Pictures/.pd_. We checked the server of the SCADA system (WinCC Explorer 7.2 installed), and we also republished the site. Then, we checked the antivirus and Pictures folder and fixed the error in the Pictures folder. However, the issue persisted and the site is still loading very slowly, and when it is loaded the connection to the server is lost when the clients attempt to perform any action.
|
Follow us on