10/13/2016 12:13 PM | |
Joined: 2/27/2014 Last visit: 6/14/2024 Posts: 689 Rating: (199) |
Hello, Best way to generate TCON_IP_v4 data block, Insert the TCON block in one of the network. Go to the configuration part of TCON block and generate the connection DB. Once connection DB is generated then delete the TCON block and its instance DB. The same connection DB can be used for connect para to MB Server block. Do the passive connection. see the attached video for generating connect DB. If you feel this post is useful then don't forget to rate. AttachmentTest.zip (884 Downloads) |
With Best Regards, |
|
This contribution was helpful to5 thankful Users |
Follow us on