7/15/2022 4:02 PM | |
Joined: 9/27/2006 Last visit: 11/18/2024 Posts: 12296 Rating: (2691) |
Hello Rolf; You can do this type of cnnection either using a CP 443-1 or directly on the integrated profinet port of the CPU, your choice. There are two links, one for each option, both provide access to sample programs that you can use as a basis for your own program (in Simatic Manager): - How do you configure a TCP connection for data exchange between S7-300 and/or S7-400 by way of Industrial Ethernet CPs? https://support.industry.siemens.com/cs/us/en/view/22385024 - How do you program the communication blocks FB63 "TSEND", FB64 "TRCV", FB65 "TCON" and FB66 "TDISCON" in order to use the TCP protocol for data exchange by means of the integrated PROFINET interface of an S7-300/S7-400 CPU? https://support.industry.siemens.com/cs/us/en/view/29737950 Hope this helps, Daniel Chartier |
This contribution was helpful to1 thankful Users |
Follow us on