3/28/2023 3:09 AM | |
Joined: 10/24/2022 Last visit: 5/29/2023 Posts: 1 Rating: (0) |
Hi Guys, I have the same issue but I'm trying to find the IP address of a S7-300 but am using S5/S7 for windows by IBH softec. Does anyone know of a way to do this? Cheers, Brock Turner ------------------------------------------------------------------------------------------ |
Last edited by: Jen_Moderator at: 03/28/2023 11:30:20New subject after splitting |
|
3/28/2023 4:25 AM | |
Joined: 3/30/2020 Last visit: 10/14/2024 Posts: 4872 Rating: (996) |
Sounds to me as if you are in the wrong place. Would the people who supply the software not be better suited to answer your question? There is a free piece of software that is recommended because of its 'talent' to analyze a network. It is useful to have regardless of which software is used to engineer the PLC. Have a look at LINK: PRONETA Basic 3.5 Commissioning and Diagnostics Tool for PROFINET |
Last edited by: qwazee at: 03/28/2023 04:26:31Activities of this user is voluntary. There is no obligation or liability placed on this user. Though optional, your 'please' and 'thank you' is highly valued. |
|
4/14/2023 9:36 AM | |
Joined: 4/28/2015 Last visit: 2/7/2024 Posts: 10533 Rating: (821)
|
Hello,
in this case that some specific gateway is used, you need contact IBH for other useful diagnostic option. This Gateway's IP can be also find on PG/PC interface inside its option in case of MPI/DP connection profile because IP address I expect there as Gateway IP configured. Your question is little bit confusual because you can easy also find IP of S7-300 via this Gateway in case of diagnostic under TIA SW. I jusr answer this as I expect general functionality because it's also not clear to me exactly what IP of what exactly device you're looking for although S7-300 is mentioned and not exactly ETH port interface is specified. |
With best regards... |
|
Follow us on