10/29/2020 3:21 PM | |
Joined: 9/27/2006 Last visit: 6/26/2024 Posts: 12262 Rating: (2672) |
Hello AOA94: I imagine you would get a system error attempting to connect Profibus-DP devices to S7-1500H/R CPUs to establish redundancy. The S7-1500 R/H system uses Profinet connectivity with MRP ring topology to connect to redundanct IO devices and between the redundant CPUs. See the screenshot below, taken from the S7-1500R/H system manual: SIMATIC S7-1500 S7-1500R/H redundant system https://support.industry.siemens.com/cs/ww/en/view/109754833 The technical term for the type of redundant connection is S2; you will find explanations for the different types of Profinet redundant connections in this article: Profinet University: Redundancy Terms: S1, S2, R1, R2 https://profinetuniversity.com/system-redundancy/redundancy-terms-s1-s2-r1-r2/ You will have to rethink the design of your application it seems. Hope this helps, Daniel Chartier |
Last edited by: dchartier at: 10/29/2020 15:24:43 |
|
10/30/2020 6:10 PM | |
Joined: 8/7/2017 Last visit: 1/7/2024 Posts: 7 Rating: (0) |
Hello Daniel Chartier, Thank you for your help! I have seen the document and I built the structure base on it, but I'm wondering how Siemens offer a new redundancy solution without adding a solution that cover and enables us to communicate with Dp-slaves! Regards, |
Last edited by: AOA94 at: 10/30/2020 18:12:18 |
|
10/30/2020 8:01 PM | |
Joined: 9/27/2006 Last visit: 6/26/2024 Posts: 12262 Rating: (2672) |
Hello AOA94; Siemens does propose a way to integrate DP slaves in a S7-1500R/H ring, theough a PN/PN coupler and a secondary Profinet controller (with an additional DP master CM or CP).This allows S2 reduncancy throughout the Profinet ring, and adds acess to the DP slaves data. It might look contrived, but not much more than the design of a Y-link, in a S7-400H system. See this article: How do you operate DP slaves on a redundant S7-1500R/H controller? https://support.industry.siemens.com/cs/ww/en/view/109771853 Hope this helps, Daniel Chartier |
This contribution was helpful to3 thankful Users |
Follow us on