5/2/2009 7:05 PM | |
Joined: 4/8/2009 Last visit: 5/22/2024 Posts: 35 Rating: (1) |
OK I didn't expect a response so fast :) I can only add one picture here!! :( Here is the next one. |
5/2/2009 7:09 PM | |
Joined: 4/8/2009 Last visit: 5/22/2024 Posts: 35 Rating: (1) |
So, now we should be OK. again thanks in advance Regards Cem
|
5/2/2009 8:07 PM | |
Joined: 4/8/2009 Last visit: 5/22/2024 Posts: 35 Rating: (1) |
Hi, I've attached the configuration file below. IMPORTANT!!! I got an error while Uploading the attachement. so please change the extension to .zip ! ! !
AttachmentWireless.pdf (120 Downloads) |
5/2/2009 8:34 PM | |
Joined: 4/6/2006 Last visit: 2/5/2024 Posts: 604 Rating: (56) |
Hi, The only reason I can think off is a defect cable or a problem with the cabling. Is the same connector used every time or did you used new connectors? Furthermore I've checked your configuration files. I don't see failures but I can give you some advice to enhance your system. 1. You use 802.11h I wonder why you have chosen for this. Is it an outside application? Are all the channels available for 802.11a blocked by other systems? 2. Please choose a different alternative channel. Here I would advice zou to use channel 140. 3. Update your firmware to version 4.1.11. Do not use 4.1.18 because with this version the 802.11h channels are blocked. This is only temporarily. Download of Firmware Update V4.1.11 for SCALANCE W-700 4. You could check what happens with your connection if you change the MAC Mode of the Client to Layer2Tunnel. You don't use PN IO Traffic since your are talking about PUT/GET but you have a PN IO System in your HW-Config otherwise your BF2 LED won't lit up when the cable is gone. 5. Did you already exchanged the CPU's for a time to check or the behaviour is only there where the WLAN Client is involved. 6.I would love to get feedback when you solved the problem. |
Best regards, |
|
Follow us on