2/19/2020 4:24 PM | |
Joined: 10/5/2016 Last visit: 2/19/2020 Posts: 1 Rating:
|
Dear Colleagues, Which Version of Windows 10 is allowed to use? Is LTSB/LTSC supported? Greetings Thomas ------------------------------------------------------------------------------------------ |
Last edited by: Jen_Moderator at: 02/20/2020 12:39:12New subject after splitting |
|
2/20/2020 2:01 PM | |
Joined: 6/4/2010 Last visit: 8/5/2024 Posts: 386 Rating:
|
Dear forum member, Desigo CC V4.0/V4.1 basically supports all the Windows 10 Professional and Enterprise versions. Only Windows 10 Enterprise provides the LTSC (Long Term Servicing Channel) feature. See LTSC: What is it, and when it should be used. Windows 10 Enterprise 2019 LTSC corresponds with the Windows 10, Version 1809. Therefore the short answer: yes, LTSC is supported, of course. Please note that the tests for the latest feature updates are a bit delayed. The test for the latest Windows 10 feature update 1909 runs currently. There are no issues known so far. Best regards, Albis |
Follow us on