11/16/2018 11:00 AM | |
Joined: 1/9/2018 Last visit: 1/12/2024 Posts: 52 Rating: (1) |
I have selected the latest Modbus versions (4.2) and i am still seeing the same error message - block not supported in this CPU. I have TIA V15 and the CPU is V2.5 of CPU1516 3-PN/DP. This text is from the help in TIA "As of instruction version V4.0 of Modbus_Slave and as of firmware versions V2.5 (S7-1500 CPUs) or V4.2 (S7-1200 CPUs), you can access data areas in DBs instead of directly accessing process images and holding registers" ------------------------------------------------------------------------------------------ |
Last edited by: Jen_Moderator at: 11/16/2018 1:30:13 PMNew subject after splitting |
|
11/19/2018 9:55 AM | |
Joined: 6/19/2017 Last visit: 5/3/2024 Posts: 8006 Rating: (163) |
Closed cause question posted twice. The second thread with the subject Modbus_Slave V4.2 - Which CPU is supported? is published within the conference Communication / Networks.
Jen_Moderator |
My Forum is the place to personalize your profile, |
|
Follow us on