1/19/2024 12:21 PM | |
Joined: 5/6/2022 Last visit: 5/9/2024 Posts: 419 Rating: (82) |
hi I have a few questions about your question in the post: - Does it happen to you with one client or with all clients? - Do you have a separate bus for the plant and terminals? - How have you started the clients, through simatic shell or directly from wincc explorer? - Are all devices visible in Simatic Shell? I also recommend that you review the following FAQ so that you can verify that you meet all the requirements: "What are the requirements for operating SIMATIC WinCC in a Windows network?" Best regards! |
Last edited by: ElonksuM_SN_BN at: 01/19/2024 12:21:30If this Information really helps, you could use the Rate function |
|
2/2/2024 9:44 AM | |
Joined: 8/3/2009 Last visit: 5/13/2024 Posts: 12933 Rating: (1646)
|
Hello Caleksey I think Upd4 is the latest/last for V7.5 without SP the lmhosts shoudl be created on each WinCC station, theoretically this should lead to a 100% working name resolution (it is needed for SQL Server and so on ). If you have a working DNS Server in the network and the name resolution does work then It should also work without it (but if you have an interruption to the DNS there is no name resolution) perhaps this FAQ helps also: https://support.industry.siemens.com/cs/de/en/view/35840700 Bye Murof |
If this Information really helps, you could use the Rate function |
|
Follow us on