11/18/2016 2:41 PM | |
Joined: 4/21/2015 Last visit: 4/19/2022 Posts: 18 Rating: (0) |
Dear All, Need a solution for the below issue: i am using siemens 1500 cpu with profinet communication and 3 nos of 1500 IM . 1 no of IM is located with the cpu while another 2 IM;s are in remote panel 1 and 2 respectively. All the modules are on profinet communication. now for testing purpose i have connected my CPU and 1st IM using profinet cable and my 2nd IM, 3rd IM again by profinet. now i am trying to patch the 1st IM and 2nd IM with lotus wireless but not able to do the hardware communication.The CPU is going faulty with "IO device not accessible" I am able to ping all the devices from both end also in TIA portal Accessible nodes i am able to see all the devices. Any idea on the issue. thanks in advance ------------------------------------------------------------------------------------------ |
Last edited by: Min_Moderator at: 11/18/2016 3:55:21 PMNew subject after splitting |
|
7/3/2017 11:33 AM | |
Joined: 2/4/2015 Last visit: 7/26/2023 Posts: 64 Rating: (0) |
Hi, I am also facing a similar problem. Have you got any solution? Regards Surendhar M |
Follow us on