8/6/2020 1:40 PM | |
Joined: 5/1/2016 Last visit: 8/6/2025 Posts: 20 Rating:
|
Hello How do I download simosim V5.3 without downloading of all the scout back? I have already installed simotion scout V5.3.1.0, but without the SIMOSIM component. ------------------------------------------------------------------------------------------ |
Last edited by: Jen_Moderator at: 08/06/2020 14:21:36New subject after splitting |
|
8/6/2020 2:16 PM | |
Joined: 5/12/2006 Last visit: 9/15/2025 Posts: 22710 Rating:
|
not possible. |
8/7/2020 12:30 PM | |
Joined: 10/11/2006 Last visit: 9/15/2025 Posts: 6040 Rating:
|
Hello the SIMOSIM Button is active if the version which is installed is the same as in your project. Link download SIMOSIM: https://support.industry.siemens.com/cs/ww/en/view/109766964 You can install different versions from SIMOSIM (V5.1/5.2/5.3) on the same PC. SIMOSIM supports Devices D4x5-2 |
With best regards, |
|
8/7/2020 5:17 PM | |
Joined: 5/1/2016 Last visit: 8/6/2025 Posts: 20 Rating:
|
thanks, it's already working.
|
8/7/2020 5:24 PM | |
Joined: 5/1/2016 Last visit: 8/6/2025 Posts: 20 Rating:
|
As a suggestion I think I could have separately, the SimoSim folders are inside volume 2, and have installers only for the application, in my case, I had to remove ScoutSimulation externally, through windows.
|
Follow us on