3/18/2014 10:09 AM | |
Posts: 10 Rating: (0) |
Please suggest me a Siemens PLC model that is compatible with the controller whose manual is attached below so that it can be used as an interface between the controller and a remote SCADA system having Modbus RTU connectivity.AttachmentDAC-Quad-Manual.pdf (90 Downloads) |
3/18/2014 12:39 PM | |
Posts: 10 Rating: (0) |
I have selected a siemens PLC can anybody tell me whether this is suitable for acting as interface between Dmx controller and Scada having Modbus RTU.AttachmentS7-1211C.pdf (87 Downloads) |
3/19/2014 6:24 AM | |
Joined: 3/20/2013 Last visit: 4/3/2024 Posts: 676 Rating: (44) |
For serial communication with S7-1200 you need also the CM1241, RS232 6ES7241-1AH32-0XB0. if you use a S7-1500 there is a CMPtP for seriel communication. With S7-300 you can use the CP340/CP341 |
Best Regards, |
|
Follow us on