(0)| 2/7/2011 10:24 AM | |
|
Posts: 2 Rating:
|
Hi, how can I add max Network on logo. I add 16 network and I can't add new network, |
| 2/7/2011 10:50 AM | |
|
Posts: 173 Rating:
|
If I understand you correctly, you want to have more OUTPUTS from the LOGO! (you have used PLC 'Ladder' programming terminology) The LOGO! can only address a MAXIMUM of 16 digital outputs. Even if you add more expansion modules, you cannot have more outputs in the program. If you add 4 x DM8 or 2 x DM16 expansion modules, you cannot even use the last 4 physical outputs on these modules - the LOGO! program just cannot address them. There are some ideas on the Forum of how to work with some more outputs - I posted an idea in this direction, but I cannot remember the link to it - maybe search for 'more outputs" in the search field above. /tf/WW/en/Posts/38357 Cheers |
Last edited by: LOGO!Barbarian at: 2/7/2011 10:53 AMJust added the link I found, but looks like Audrey found it first! |
|
This contribution was helpful to
|
|
| 2/7/2011 10:56 AM | |
|
Posts: 2930 Rating:
|
Hi, what do you mean with 16 Network? LOGO! supports up to 16 Outputs but no network. Helmut |
| 2/7/2011 12:24 PM | |
|
Posts: 2 Rating:
|
Network mean not output. network mean line. I find it. thanks |
| 2/7/2011 2:14 PM | |
|
Posts: 153 Rating:
|
The information about communication modules of logo here |
Follow us on