7/12/2012 12:40 PM | |
Posts: 267 Rating:
|
Sorry, but there is no attachment. Do you have some more information about your problem? |
7/12/2012 5:26 PM | |
Posts: 267 Rating:
|
Check your PG/PC Interface settings: Start->Settings->Control Panel->Set PG/PC Interface Access Point of the Application: S7ONLINE (STEP 7) Interface Parameter Assignment Used: TCP/IP or TCP/IP(Auto) -> "your network card" If your network card isn't listed, install it via "Select..." or try with the S7-1200 Tool: http://support.automation.siemens.com/WW/view/en/41737436 |
7/13/2012 4:41 PM | |
Posts: 267 Rating:
|
Hello, I think/hope yournetwork cardis in the same subnet (mask: 255.255.255.0)as your S7-1200. so it has an IP address like: 192.168.0.x I wonder if the cable is broken. Do the LEDs (RUN/STOP, ERROR, MAINT) of the S7-1200 tell anything? http://support.automation.siemens.com/WW/view/en/36932465chapter 14.1 Do you know which firmware should be on it or do you have a MC card to delete the CPU or make a firmware update? http://support.automation.siemens.com/WW/view/en/40588092 http://support.automation.siemens.com/WW/view/en/41886031/133100 |
Follow us on