1/25/2016 6:46 AM | |
Joined: 4/23/2010 Last visit: 11/23/2024 Posts: 8092 Rating:
|
Hello, This is 611-Analog drive, 80/160 A enhanced interface feed module. If fault is sporadically reset it or if it is permanent, significance of fault code 7 is motor feeder cable interrupted or motor cable short circuit or ground fault etc. If every thing is Ok, then control module is faulty, replace the same. Please refer attached sheet. |
1/26/2016 8:18 PM | |
Posts: 50 Rating:
|
Thanks for the help, the drive was the cause of the fault. |
This contribution was helpful to
1 thankful Users |
Follow us on