6/24/2018 7:39 PM | |
Joined: 9/27/2006 Last visit: 9/15/2025 Posts: 12408 Rating:
|
Hello Mirip; To add to Dan's (#dP) post, the base (starting address of the S7-200 analog modules is determined by their position next to the CPU, and the number of analog modules preceding them. This is explained vey well in this FAQ, and in the S7-200 System manual, in the section PLC Concepts. Which addresses do the S7-200 input/outputs of the S2-200 expansion modules receive? https://support.industry.siemens.com/cs/ww/en/view/24122845 S7-200 System manual: https://support.industry.siemens.com/cs/ww/en/view/1109582 I hjave tried to illustrate this concept in the following attachment; if the base address of the module is AW8 (for example), then each analog input circuit follows: AW10, AW12... AW22 Hope this helps, Daniel Chartier |
Last edited by: dchartier at: 6/24/2018 8:27:17 PM |
|
6/24/2018 9:16 PM | |
Joined: 6/14/2013 Last visit: 3/18/2023 Posts: 218 Rating:
|
Thanks #dP and dchartier, but here is my problem in image: Best regard, mirip |
Follow us on