7/11/2019 1:01 PM | |
Joined: 6/29/2018 Last visit: 8/28/2025 Posts: 23 Rating:
|
DCC can not write to drive parameter p320 Motor-Bemessungsmagnetisierungsstrom The p320 is not offered in the list when "Verschaltung zu Operand" is selected from a real output. The list starts with p480, no smaller numbers. Background: In case of low torque output in torque controlled mode, the torque output jumps between 0.5 Nm and 0.9 Nm on a 1PH8 that is rated 39Nm. ------------------------------------------------------------------------------------------ |
Last edited by: Papa123 at: 07/11/2019 13:06:05Last edited by: Jen_Moderator at: 07/11/2019 14:50:07New subject after splitting |
|
Follow us on