2/19/2025 12:51 PM | |
Joined: 8/10/2012 Last visit: 2/25/2025 Posts: 3 Rating:
|
We have tried to configure the DIRIS A40 SOCOMEC Multifunctional meter (P/N- 48250502) with S7 1517F-3PN/DP PLC System. We have used the GSDML "diri0948v3" in the HW Config , but we are not able to reach the Meter over Profibus. The Meter is a DPV1 slave and in the HW Config the Master is set to DP V0 by default (with no provision to change it). The meter is connected to the X3 port of the PLC S7-1517F-3PN/DP, the other ports are occupied with PROFINET slaves. The meter is working is good on the panel, the PROFIBUS settings are already set in the meter, we have tried with multiple bandwidth and with no success. The meter is just not able to be integrated with the PLC and hence the values are not able to read on the SCADA. Thanks, Prasanth Attachmentdiri0948v3.zip (184 Downloads) |
Follow us on