6/5/2012 8:27 AM | |
Posts: 205 Rating:
|
Hi Expert, i want to know how to add SIEMENS Drive in s7-1200 PLC project??? |
6/5/2012 8:34 AM | |
Joined: 5/12/2006 Last visit: 9/15/2025 Posts: 22710 Rating:
|
Hello, you must install the GSD file for the drive. Regards Christoph |
6/5/2012 8:42 AM | |
Joined: 8/31/2010 Last visit: 7/18/2025 Posts: 1525 Rating:
|
Hello sparten, refer this, which is one of the option Connecting a SINAMICS drive to an S7-1200 CPU in TIA Portal (via GSD file) the other option is using StartDrive v11 software. |
Like it? Rate it! |
|
6/5/2012 8:48 AM | |
Joined: 4/24/2009 Last visit: 8/20/2024 Posts: 2682 Rating:
|
Thread closed, because question is already published in the following thread LIBRARY FOR S71200MPLC ON USS COMMUNICATION WITH MM420 DRIVE. Best regards O_Moderator |
Follow us on