3/15/2023 12:28 PM | |
Joined: 1/21/2013 Last visit: 9/8/2025 Posts: 4093 Rating:
|
Hi christopherreyes, Yes, I have tested the event and it works. I had to install SIMATIC WinCC Unified PC, V18.0 Upd1 SR1 to test it in simulation. Kind regards |
This contribution was helpful to
1 thankful Users |
3/15/2023 3:07 PM | |
Joined: 1/10/2023 Last visit: 5/27/2025 Posts: 60 Rating:
|
Hi Stefan, I have installed that update and I tested the "Input finished" event with a WinCC Unified PC RT and I still can't get it to work. I'm starting to think that maybe I don't understand when the event is executed. From my understanding, the event is executed when, for example, you press the "enter" key after entering a value in an IO Field. Could you share an example project with me? Thank once again. |
3/16/2023 7:08 AM | |
Joined: 1/21/2013 Last visit: 9/8/2025 Posts: 4093 Rating:
|
Hi christopherreyes, In the attached ZIP file you will find the project I tested with and a video showing the results. It's a very simple HMI project with only one internal variable, one IO field and a circle next to this field. When a new value is entered into the field, the color of the circle changes. Kind regards AttachmentInputFinished.zip (677 Downloads) |
This contribution was helpful to
1 thankful Users |
3/17/2023 9:06 AM | ||||||||||
Joined: 1/10/2023 Last visit: 5/27/2025 Posts: 60 Rating:
|
Hi Stefan, I checked in TIA Administrator and seems I have the same versions as you. Where did you check your software installed? Thank you! |
|||||||||
3/17/2023 9:21 AM | |
Joined: 1/21/2013 Last visit: 9/8/2025 Posts: 4093 Rating:
|
Hi christopherreyes,
In TIA Portal, use the "Help > Installed Software…" menu to see an overview of the software. Scrolling down you will find the link "Detailed information about installed software" which will take you to another window where you can see some more detailed lists. You can also export all lists from there. Do you have older versions of TIA Portal (V17, V16, …) installed in parallel? Kind regards |
Follow us on