3/10/2025 3:09 PM | |
Joined: 10/11/2006 Last visit: 9/15/2025 Posts: 6040 Rating:
|
Hello, there must be a info in the diagnostic buffer of the CPU. Increasing the application cycle General info: How can you prevent a buffer overflow for OB92 eventshttps://support.industry.siemens.com/cs/ww/en/view/109766824 |
With best regards, |
|
3/12/2025 9:45 AM | |
Joined: 5/29/2018 Last visit: 3/14/2025 Posts: 46 Rating:
|
Good afternoon, but we don’t have OB91 or OB92 in our project! |
3/12/2025 9:49 AM | |
Joined: 5/29/2018 Last visit: 3/14/2025 Posts: 46 Rating:
|
|
3/12/2025 3:37 PM | |
Joined: 11/4/2011 Last visit: 9/10/2025 Posts: 276 Rating:
|
Hi there, the answer above from Technology Team was about S7-1500 motion control, but as you said in the beginning, you have an S7-317T, which is different. For general information on the timing of the PLC you have, see here: https://support.industry.siemens.com/cs/ww/en/view/30119663/50785477003 Basically all cycles are built on the DP(DRIVE) cycle, which is the cycle of the Profibus where you connected your drives and other hardware for use with motion control to this PLC. The question now is to which value this is set. Unfortunately I cannot really tell you exactly where you find this time, I'm writing this all from memory. But go into HwConfig, open the settings of the DP(DRIVE) bus. Then in the dialog you have open now, there is some button with further settings that opens another dialog that contains the cycle time of the DP(DRIVE). Just search around a little, you'll find it. My personal rule of thumb for setting this time: Do this, to check if your cycle time was set correctly, or if this was too small anyway. If it was too small, increase it as described above, compile HwConfig, then open S7-Technology and also do a save and compile there. Then download all to the PLC again (HwConfig as well as S7-Technology). Then check if the issue appears again. On a side note: Regards, |
3/13/2025 8:05 AM | |
Joined: 11/4/2011 Last visit: 9/10/2025 Posts: 276 Rating:
|
Hi there, the set cycle time seems fine to me then. Too large is not really a problem, only too short. I only wonder about the rather large To-Time of 1ms, but again, I don't really have an idea why this should be an issue and cause such errors. My suggestion: Regards, |
Follow us on