1/12/2023 2:26 PM | |
Joined: 5/25/2015 Last visit: 9/2/2025 Posts: 4 Rating:
|
Hi, Thank You for answering. I'm not 100% OK with Yourpoint of view regarding I/O fields focus with Comfort touch-Panels. For example, I used such I/O input field for a barcode scanner connected at the USB port of a TP1500 Comfort panel. The idea was to allow the operator to scan 2 different barcodes while starting the production : - 1st barcode correpsonds to the product batch number - 2nd barcode correpsonds to the part serial number Moreover, the customer required the system to accept a random scan order from the operator (so the appliction was developped to analyse the scanned codes and determine which one have to be affected to the batch number (and therefore, the other one was affected to the product reference) as some included charcaters where intended to check this. So before the first scan, I wanted the TP1500 to be awaiting an input via the scanner (as if the focus wasn't set before on the I/O field, then the read barcode was lost). My difficulty was to set the focus on the I/O input field while awaiting scan. On this test-bench application, I've done a lot of VB Scripts to solve the different customer requests (barcodes scan, csv files generation and save them on the plugged SD-card, move these files n request from SD-card to a USB memory , check the SD-Carde free space, ...). I'm now preparing a new application and think I will use a Unified Comfort panel (I hope that all these scripts will be easier to develop, debug and maintain !...). Is there any link to Unified Comfort Panels scripts development? ------------------------------------------------------------------------------------------ |
Last edited by: Jen_Moderator at: 01/13/2023 09:01:34New subject after splitting |
|
1/13/2023 10:12 AM | |
Joined: 6/22/2020 Last visit: 5/22/2025 Posts: 120 Rating:
|
Here you have a nice document with tips and tricks for Javascript in Unified: https://support.industry.siemens.com/cs/ve/en/view/109758536 |
If this post was helpful, please rate it! |
|
Follow us on