5/2/2025 1:53 AM | |
Joined: 1/7/2025 Last visit: 5/21/2025 Posts: 2 Rating:
|
Dear, I'm configuring a SCALANCE M876-4 as an OpenVPN client to remotely access devices in VLAN1 (192.168.100.1/24). The SCALANCE is equipped with a SIM card and connects to the internet via mobile data. To make the SCALANCE reachable, I've set up dynamic DNS using No-IP. The VPN tunnel establishes successfully, and the SCALANCE receives an IP address in the 10.8.0.0/24 range (e.g., 10.8.0.6). My goal is to access the Web Based Management (WBM) interface of the SCALANCE and other devices in VLAN1, such as the PLC (S7-1510; IP: 192.168.100.10/24; Gateway: 192.168.100.1) and HMI (is a Unified Panel, IP: 192.168.100.11/24; Gateway: 192.168.100.1) connected to port 1 of VLAN1, through the VPN tunnel. However, despite a successful VPN connection, the WBM interface is inaccessible via the tunnel, and I cannot connect to the PLC and HMI. I have experimented with adding topology subnet, but this resulted in completely losing access to the WBM interface. Has anyone experienced configuring a SCALANCE M876-4 as an OpenVPN client to achieve full access to VLAN1 and the connected devices via the VPN tunnel? Any suggestions or examples of working configurations would be greatly appreciated. For more context and visual support, I've attached a Word document containing relevant screenshots of the current configuration and network status. AttachmentOpenVPN Config.zip (109 Downloads) |
Last edited by: AutoGen_3775736 at: 05/02/2025 01:56:03 |
|
5/21/2025 12:29 PM | |
Joined: 1/7/2025 Last visit: 5/21/2025 Posts: 2 Rating:
|
Thanks for the reply, I’m going to give it a try. I’ll let you know whether it worked or not. |
Follow us on