3/5/2018 8:46 AM | |
Posts: 2930 Rating:
|
Hi, can please post your LOGO! Program to check? Thanks |
3/5/2018 7:26 PM | |
Posts: 6 Rating:
|
Attached you will find the photos of the logo AttachmentlOGO.zip (920 Downloads) |
3/5/2018 7:42 PM | |
Posts: 6 Rating:
|
Hi the program is very simple, attached ypu will find it
AttachmentCircuit Diagram1.zip (894 Downloads) |
This contribution was helpful to
1 thankful Users |
3/6/2018 2:41 AM | |
Posts: 6 Rating:
|
Is important to say that this program was develop and is working in Logo 0BA7, the connections and encoder are the same but in Logo 0BA8 this program is not working. Attached you will find some videos. We test with a 25 PPR Encoder, when we move slow the encoder the count is OK But when we increase the speed, the counter move the number in a strange way. In the video SLOW_SPEED we move slow the encoder until 125 and later we start moving the encoder in reverse and the count is OK I both directions. In the video FAST_SPEED we move faster the encoder increasing in all the process but in the value 80 the counter decrease to 64, later to 90 and later to 83. The Encoder and all the cables are shielded, the frequency of the pulse are below 4 Hz AttachmentVIDEO.zip (790 Downloads) |
Follow us on