2/16/2025 1:23 PM | |
Joined: 12/24/2017 Last visit: 3/14/2025 Posts: 2 Rating:
|
Hello, I am working on a project with one sensor and 2 actuators (both set at a certain distance away from sensor, for example Actuator 1 to sensor distance is 300mm and actuator 2 to sensor is 4500mm). I am unable to track the position of the products which pass from the sensor towards these actuators. I tried using array shift using encoder pulses to shift the array value but due to higher pulses from the encoder, the PLC keeps missing pulses. I am using a S7-1212 DCDCDC. Could anyone assist me on this please? ------------------------------------------------------------------------------------------ |
Last edited by: Moderator_Lan at: 02/17/2025 10:18:31New subject after splitting |
|
2/17/2025 10:20 AM | |
Joined: 7/30/2024 Last visit: 8/29/2025 Posts: 936 Rating:
|
Topic closed because the question was posted twice. The active topic can be found here: Multiple Products Tracking on Conveyor with Rotary Encoder Kind regards, Moderator_Lan |
Follow us on