11/13/2009 7:42 AM | |
Joined: 10/7/2005 Last visit: 9/14/2025 Posts: 3049 Rating:
|
Hello Abhay I must admit I havn't used the 1POS (6ES7 138-4DL00-0AB0) card yet, but am wondering whyyou say "it will miss the pulses"if run @ 100 rpm. 2500ppr @ 100 rpm is just over 4 kHz and the 1POS card is capable of 100 kHz with a 24V incremental encoder, so i am really a bit at a loss to find an explanation for your problem. For now I can't really give you any advise, but perhaps someone else might and it would be helpful if you could advise further on your handling of the shear (e.g. are you trying to change the Setpoint whiele the shear is in operation?) and/or upload your program here. Just for completeness and in case you don't have it yet, below is the link for the ET200S positioning manual which may (hopefully) help too: ET200S Positioning manual I hope this helps (somewhat at least) |
Cheers |
|
Follow us on