12/24/2018 2:41 AM | |
Joined: 8/6/2018 Last visit: 1/6/2025 Posts: 23 Rating:
|
Hi All, Currently I'm selecting Sitrans P DS III. I just want to confirm what I'm understand measuring span listed in Sitrans configurator This means I can modify range 0 for low value and any value between 16 to 5 for high value. Span: 1 to 30 bar a (14.5 to 435 psi a), overload limit 100 bar This means I can modify range 0 for low value and any value between 1 to 30 for high value. Selection is for absolute pressure transmitter. Thank you. |
Follow us on