5/1/2023 5:25 PM | |
Joined: 8/30/2011 Last visit: 9/5/2025 Posts: 12 Rating:
|
Hi Stefan, I have a problem with V18.0.0.0 on an MTP1200 and I am hoping that it is fixed with version V18.0.0.1. If possible, can you recreate and check on new firmware + hardware. The problem does not exist with PC or simulation. When the operator touches a button, the color changes slightly with the "mouseover" highlighting. When the operator touches another button, the "mouseover" highlighting of the previous button is not updated. If the touch action is slid out of the touch area of the button, the highlighting is updated. If a mouse is used, the highlighting is updated. If the page is viewed with the web client, (served by webserver of MTP1200 and viewed at 127.0.0.1 or localhost) the highlighting is updated, however the experience is very slow. ------------------------------------------------------------------------------------------ |
Last edited by: Jen_Moderator at: 05/02/2023 04:41:49New subject after splitting |
|
Follow us on