10/9/2015 4:31 PM | |
Joined: 12/18/2014 Last visit: 9/14/2025 Posts: 35958 Rating:
|
You must create the parameters time on and time off in the corresponding message text. Then after the transfer of the program to select the appropriate message text in the logo and the logo start. If this is selected, hold down the ESC key for more than 2 seconds until a black bar appears on the display. Now you can select with the cursor up / down the appropriate field to be changed. Is selected the field, press the OK button. The cursor turns now in a blinking box. Now you can select with the cursor left / right the place which you want to change. With cursor up / down you can change the value of the place. If you have made the change, press the OK button. The cursor is now back to a black bar. With cursor up / down, you can select another field and change it again or ESC to return. AttachmentSchaltplan1.zip (386 Downloads) |
This contribution was helpful to
1 thankful Users |
Follow us on