11/26/2013 12:37 PM | |
Joined: 8/31/2010 Last visit: 6/8/2024 Posts: 1515 Rating: (223) |
The SIMATIC Memory card which is used in S7-1500 is not a typical SD card, even though it can be accessed using SD card reader.
Hello filipefs, The SIMATIC Memory card from a S7-1500 system can be used with another similar S7-1500 system by just removing the card from the first system to the similar system. For your requirement, you can download the project into a SIMATIC MC (Memory Card) and keep that as a backup card so that you can restore it on a later date. Use another SIMATIC MC which will be actually functioning with S7-1500. For more info - SIMATIC memory card - overview Hope this helps. |
Like it? Rate it! |
|
Follow us on