7/8/2012 10:01 PM | |
Joined: 7/3/2011 Last visit: 5/17/2025 Posts: 82 Rating:
|
Dear Experts, Now am working with s7 315-2DP Redundant system working in MPI, ET 200M profibus station-1 and WinCC connecting Ethernet (Individual CPU have CP 343). In my project am facing some problems as bellow, 1) I have created my project in PLC its working fine, After switch off both CPU and again on the CPU -2 (PLC-B) is active first. How its changed i cant understand. I read the related softaware manual (S7-300/S7-400Software redundancy forSIMATIC S7) mentioned following functionality should be checked A). Read the status word from sation A (DB5.DBW8). The value 1000 0000 0000 0101 should be displayed. Meaning: The station is subunit A and master; all DP slaves can be addressed. B). Read the status word from station B (DB5.DBW8): The value 1000 0000 0000 0101 should be displayed. Meaning: The station is subunit B and standby; all DP slaves can be addressed. But I have received different value from both CPUs i have attached here my VAT... I wants now how to mention PLC-A is a master. 2) IF CPU-2 is active condition the communication between WINCC its working fine. All variable can able to read and set the bits using button function also ok. If i put CPU B in stop mode , The ET-200m changed ok and wincc tag variable reading values are also ok, but i could not able to set the bits using button function also using global vb script (Using for reporting function). I have createed theRedundant connections in dynamic wizard as per the manual, also i have checked the same problem faqs but there is no answer, Please give me the solution as soon as eariler, Here I have attched VAT table diagnostics details received from the PLCs Regards RSK AttachmentNew folder.zip (272 Downloads) |
Last edited by: Strongs at: 7/8/2012 10:06 PM |
|
11/11/2012 10:25 AM | |
Posts: 7 Rating:
|
Could you please send me your program please, I have a project s7-300 redundancy Regards, Marwan |
Follow us on