1/28/2010 10:11 AM | |
Posts: 37 Rating:
|
Dear Sir, I am doing commissioning of Masterdrive at Bhushan -HSM India. Motor details are as follows: Motor Voltage: 660V Motor Current:335A Motor PF: 0.78 Motor Frequency: 50Hz Motor rated Speed: 747rpm Motor maximum speed is not mentioned on the name plate which is 940rpm I want to run the motor above base speed of 740 rpm. But in that case my motor voltage increased above rated voltage of 660V & sound also starts coming from motor. I have mentioned motor rated speed(P108)=747rpm & Ref speed(P353)= 940rpm. Motor details are also attached. How to run the motor above base speed? Thanks in advance..waiting for your reply. -Amit.. AttachmentBending drives.pdf (436 Downloads) |
7/14/2013 10:38 AM | |
Posts: 8946 Rating:
|
returning to the eve? |
7/14/2013 11:27 AM | |
Joined: 4/23/2010 Last visit: 11/23/2024 Posts: 8092 Rating:
|
Sorry but don't understand. |
7/16/2013 10:07 AM | |
Joined: 11/18/2010 Last visit: 8/5/2022 Posts: 523 Rating:
|
Be careful in this range torque limit is also decrease so if load is high it isnot recommended VP |
Follow us on