2/2/2023 10:18 PM | |
Joined: 7/31/2019 Last visit: 4/28/2023 Posts: 6 Rating:
|
Hi All, I have an existing multi-project with an AS, 1 ES, 2 redundant OS, 2 redundant Batch Servers and 4 clients. I am in the process of adding another project under this multi project which will share all the servers, but will have its own dedicated AS. The problem I am facing is that when I am trying to update the Process cell, the 2nd AS is not showing up and hence updating and downloading the process cell only updates the units related to the old AS but nothing is available from the new AS. What needs to be done to update the process cell with the Units from the new AS. Screen shots of the architecture and what I am seeing inside the Configure Batch Window is attached. Any insight will be much appreciated. Thanks.
AttachmentScreenshots.pdf (445 Downloads) |
2/3/2023 11:36 AM | |
Joined: 8/1/2019 Last visit: 9/1/2025 Posts: 304 Rating:
|
Have you merged the new AS Network in the Netpro? |
2/3/2023 8:21 PM | |
Joined: 7/31/2019 Last visit: 4/28/2023 Posts: 6 Rating:
|
Yes the new AS network has been merged in the Netpro. |
Follow us on