1/28/2016 10:29 AM | |
Posts: 6 Rating:
|
Hi all forum members. I am now working a small Project with siemens PLCs (s7-300), and it is my first experience with siemens hardware and software. The problem is that the CPU315-2DP and CP 343-1 is showing bus failure towards the rio unit IM151-1. I have been searching this forum, and today connected my TIA portal v13 to the plc, and saved the Diagnostics buffer file. I could read the Diagnostics, but where not able to go online to read the program, not sure if it is because of tia portal, or that the plc is fucked. So now I am wondering if anybody can help me understand the errors that is showing. This PLC was delivered and programmed in year 2010 approximetly. One other problem is that I aonly have tia portal v13, and the plc program is programmed With step7 v5.x, so I cannot open the Source code in tia portal v13. Here is the Diagnostics: Diagnostics buffer of the module 6GK7 343-1EX30-0XE0 [192.168.178.30] [CP 343-1]
Best regards Morten AttachmentDiagnostics28.01.16.txt (361 Downloads) |
1/28/2016 1:51 PM | |
Posts: 6 Rating:
|
Thanks for the explanation and advises. I will lokk into this tomorrow, after TIA is updated to newest service pack. Best regards Morten |
Follow us on