8/20/2022 2:55 AM | |
Joined: 10/17/2007 Last visit: 9/15/2025 Posts: 4452 Rating:
|
Actually I want to suggest you post a new topic to SINUMERIK , USING TITLE: " 840dI CONTROLLED MACHINE 611a DRIVE all axis have error "7" I attached manual for SIMODIVE 611A, You can read section VS/xxx/. try test drive yourself , tips , release some axis motor from mechanical --free the motor. then enable 63, 64, 48 ,112 (connect to Ter. 9 (internal DC24V) then CONNECT 65,663 on 611A card, using battery conic 56/14 to see motor can run. also if you need help you need provide detail of the machine--what is happen for the month
AttachmentIAA_1000_en.pdf (594 Downloads) |
Last edited by: nulizhang at: 08/24/2022 21:06:20Last edited by: nulizhang at: 08/24/2022 21:07:28replaced with correct manual 611A (I loaded 611D) If you like my comments please |
|
8/20/2022 5:37 AM | |
Joined: 4/23/2010 Last visit: 11/23/2024 Posts: 8092 Rating:
|
Hello JEYAPRAKASH SP, If during power down of analog drive if power supply is interrupted then in such case data could not be saved successfully & F-07 alarm pops up during next power ON. Try to restart drive by setting p52=1 i.e. restart with data save mode. If it could not help, try to restore data from external device. Hope this helps. |
8/24/2022 12:29 AM | |
Joined: 10/17/2007 Last visit: 9/15/2025 Posts: 4452 Rating:
|
Hi, PISCEAN, this user did not response to my answer. --do you think he using SINAMICS drives so there will be p52=xx and F-07? @ Jeyaprkash sp, please share the picture of your drive with error
|
Last edited by: nulizhang at: 08/24/2022 03:41:27Last edited by: nulizhang at: 08/24/2022 03:44:45If you like my comments please |
|
8/24/2022 4:38 AM | |
Joined: 4/23/2010 Last visit: 11/23/2024 Posts: 8092 Rating:
|
Hello, User has mentioned 611A drive & it is possible with ADI4 module. No Sinamics drive. |
8/24/2022 8:08 PM | |
Joined: 10/17/2007 Last visit: 9/15/2025 Posts: 4452 Rating:
|
So I think he useS 611A feed drive, user friendly interface , "7" error --"Speed controller at its endstop" --I already let user post picture, and suggest all axis have "7" error --mean motor not moving at all , possible power supply DC bar not connected So there will no P52=? and no F-07 , 611A spindle drive? and I am not familiar with 840Di SL -- what the drive solution 840Di PL using 611U (via PROFIBUS)
|
Last edited by: nulizhang at: 08/24/2022 20:10:40Last edited by: nulizhang at: 08/24/2022 20:11:03If you like my comments please |
|
9/1/2022 11:00 AM | |
Joined: 10/5/2011 Last visit: 8/28/2025 Posts: 14 Rating:
|
control card doesn't have parameterizing option. Parameter board for motor selection & tacho, gain, drift setting. Attached Picture.
|
Follow us on