5/19/2008 1:41 PM | |
Joined: 5/13/2008 Last visit: 12/18/2019 Posts: 836 Rating:
|
The function “SetAcousticSignal” configures the acoustic feedback of touch screen operation. This means, only operations at the touch screen can trigger this signal. For further informations refer to chapter 6.5.7, Set Volume: http://support.automation.siemens.com/WW/view/en/23337820 So, this function just controls the settings of the buzzer volume, but cannot trigger the buzzer. The function is only available on 277-Touch-Panels or higher. It looks like, you have to use an external buzzer, triggered by PLC. |
mfG / Best regards |
|
Follow us on