8/23/2024 9:26 AM | |
Joined: 11/13/2018 Last visit: 8/28/2025 Posts: 91 Rating:
|
Hello geri036, I know it's been a while, but I'm having the same problem. I only get to see maximum 100 rows. While there are more than 100 in my log. You wrote that after removing the filter, nothing changes. Were you still only getting 100 alarms? ------------------------------------------------------------------------------------------ |
Last edited by: Moderator_Lan at: 08/27/2024 08:34:53New subject after splitting Like it? Rate it! |
|
8/27/2024 5:29 AM | |
Joined: 1/21/2013 Last visit: 9/11/2025 Posts: 4102 Rating:
|
Hi MindFlayer,
When viewing logged alarms, you can choose between two viewing modes:
If only logged alarms are to be shown, 1000 can be displayed. If the logged alarms are also to be updated, the limit is set to 100. See the manual for details. Kind regards |
This contribution was helpful to
1 thankful Users |
9/12/2024 5:49 AM | |
Joined: 11/13/2018 Last visit: 8/28/2025 Posts: 91 Rating:
|
Thank you Stefan! |
Like it? Rate it! |
|
Follow us on