7/22/2025 9:00 AM | |
Joined: 8/3/2009 Last visit: 9/5/2025 Posts: 16349 Rating:
|
Hello Jame_DI_CS If you want to migrate a project including the old archive data you should do this by copying the whole project folder including all archive data. Then open this project in WinCC V7.2/V7.3 and do a conversion of the peoject data. then you can open it also in V8.0 and do the same. This should keep all existing archive data also if you start the project in V8.0 (General information about migration you find HERE) If you copy the segments to the common archiving then the segments will be attached additionally to the normal running taglogging and alarm logging. So this could cause performance issues and should not be used with too much segments and also not permanently. Only copying the segments from one Archivemanager folder would be only the half job. There are also databases for managing wihch archive files are loaded. Check out this FAQ -> But the first way would be the best |
If this Information really helps, you could use the Rate function |
|
Follow us on