7/7/2024 10:47 AM | |
Joined: 1/27/2009 Last visit: 9/3/2025 Posts: 173 Rating:
|
Is that what you are looking for? |
The only thing necessary for the triumph of evil is for good men to do nothing |
|
7/9/2024 5:35 PM | |
Joined: 6/29/2024 Last visit: 4/27/2025 Posts: 41 Rating:
|
Hi, i want to use 8 inputs in binary mode, as far as i know that gives me 64 combinations. i"ve made a start with my program to see if it works. i know that it is pretty basic but this i a start for me. in the attached file there is a sample. maybe somebody can have a look at it at give me some tips/example what can be better/easyer.
AttachmentWS_Parc_V.0010_8-4-2023 with_Lamps.zip (598 Downloads) |
7/13/2024 6:08 PM | |
Joined: 1/27/2009 Last visit: 9/3/2025 Posts: 173 Rating:
|
No, you do not need to add CTUD as those two instructions do the job. One - ADD - increments value on drive in, another one - SUB - decrements the value on drive out.
AttachmentCUCD.zip (476 Downloads) |
The only thing necessary for the triumph of evil is for good men to do nothing |
|
This contribution was helpful to
1 thankful Users |
7/14/2024 6:44 AM | |
Joined: 12/18/2014 Last visit: 9/9/2025 Posts: 35938 Rating:
|
Maybe the attachment helps you. AttachmentBITSUM.pdf (485 Downloads) |
This contribution was helpful to
1 thankful Users |
Follow us on