11/23/2009 9:49 AM | |
Joined: 7/8/2009 Last visit: 6/7/2025 Posts: 1977 Rating:
|
Dear Experts, I have apllication of Exhaust fan which is controlled by analog input setpoint from DCS control. Its running in SLVC mode. V/F is not possible because it was drawing very high current. Now my problem is that, when ever any change in setpoint is occur, current is fluctuating very high. For example, setpoint is changed to 25% to 35 %, at that time, current will go from 72 amp to 130 or some times 150 amp and then bect to 75-80 amp. Due to this fluctuation, we can not run VFD in auto mode. I uploaded parameter file. Any suggestions?? Please give reply ASAP Regards, Devesh Vithani Attachmentexhaust.pdf (419 Downloads) |
Last edited by: Vithani at: 11/23/2009 9:51 AMI dont Like people driving Fast, thats the reason I overtake them ;) |
|
3/12/2013 7:32 AM | |
Joined: 6/19/2008 Last visit: 9/5/2025 Posts: 8 Rating:
|
Hi Vithani, AttachmentD:\temps\SLVC.pdf (403 Downloads) |
7/7/2013 3:44 AM | |
Joined: 7/8/2009 Last visit: 6/7/2025 Posts: 1977 Rating:
|
Hello Wow's Perhaps your problem might have solved now.. But i did manual Tunning for speed controller with load. Changed gain and time parameters, checked its effect and set to best possible values Regards, Devesh |
I dont Like people driving Fast, thats the reason I overtake them ;) |
|
Follow us on