9/15/2021 6:57 AM | |
Posts: 1 Rating:
|
I have a cut in profibus cable can i weld it ? And the amount of datq is huge ------------------------------------------------------------------------------------------ |
Last edited by: Jen_Moderator at: 09/15/2021 09:31:25New subject after splitting |
|
9/15/2021 8:33 PM | |
Joined: 4/28/2015 Last visit: 4/19/2025 Posts: 10876 Rating:
|
Hello,
if I will be at your side, I'll do this thing what I see better and somehow correct. In place of cut I set on both sides PB connectors, one with PG socket and connect sides together. |
Last edited by: Duris_I at: 09/15/2021 20:38:07Last edited by: Duris_I at: 09/15/2021 20:39:21With best regards... |
|
9/15/2021 9:19 PM | |
Joined: 9/27/2006 Last visit: 9/4/2025 Posts: 12397 Rating:
|
Hello Engs7s; Basically, any change in cable capacitance will make Profibus transmissions difficut and untrustworthy. And there is a great risk of modifying the cable capacitance at the soldering or welding point. The elementary recommendation from Profibus International (PI) would be to run another length of Pofibus cable, to re-establish a consistent connection between Profibus nodes,. If ths is not possible, look at this extract from PI's Profibus installation Guidelines proposes various suggestions to repair a damaged cable: http://verwertraining.com/wp-content/uploads/Installation-Guide-V13-small.pdf Hope this helps, Daniel Chartier |
This contribution was helpful to
2 thankful Users |
Follow us on